The highest level of physical protection for POS terminals – with the help of 3D-MID

Point-of-sale terminals (POS) are not sufficiently protected against physical attacks. Attacker can access sensitive data (such as credit card number and PIN codes) using probes or mini-drills. An additional security element in the security caps of the terminals can reliably prevent such attacks.

Acccording to a survey by the Bitkom digital association, cyber attacks have caused damages of 102.9 billion euros throughout 70 percent of companies in Germany in recent years. According to this survey, the scope and quality of the attacks have increased drastically. "The recreational hackers of the past have evolved into well-equipped and technologically savvy cyber gangs," Bitkom reports. POS terminals count among the targets. Sensitive data such as credit card numbers and PIN codes are temporarily stored on POS terminals to prevent data loss in the event that the payment process is interrupted. This data can be read by attackers if they gain access to the hardware using probes or mini-drills. An additional security element can be used which reliably prevents data loss.

POS terminals are considered a popular target for data theft. Attackers use mini-drills to gain access to credit card numbers and PIN codes.

3D-MID security caps increase the safety classification

Electrical paths (traces) on the inside of the protective cap provide a very reliable additional security mechanism that protects against physical attacks. These traces form a closed circuit. They are so close together that it is practically impossible for an attacker to gain access. Any attempt to attack would either damage a trace and break the circuit or short out two traces. This causes the POS terminal to shut down immediately, resulting in the loss of cached data and rendering the device unusable.

3D-MID caps from HARTING protect the electronics mechanically and electronically from unauthorized access. A high-precision meandering structure detects even the smallest intrusion – thus preventing data theft.

The electrical traces are applied directly to the plastic parts of the security caps using the 3D-MID process. HARTING is the largest supplier of 3D-MID components (Mechatronic Integrated Devices) outside of Asia and offers all steps in the 3D-MID process under one roof. The injection-moulded circuit carriers replace conventional solutions that use a plastic carrier and printed circuit board. They do this by integrating the function of both parts into one MID. This reduces weight, reduces the number of components and lowers production costs, while at the same time improving security. This 3D-MID solution is particularly useful for POS terminals to improve security standards and to defend against hacker attacks.

Very small trace gaps improve security

Thanks to HARTING's 3D-MID technological edge, customers benefit from compliance with the strictest PCI-DSS (Payment Card Industry Data Security Standard) requirements. This solution differs from other suppliers of safety enclosures in that it has smaller trace widths. The closer the distances between the individual traces, the more difficult it is to manipulate the circuit from the outside.

While most suppliers today can implement trace widths and spacings of around 300 to 500 µm, HARTING offers 70 to 150 µm.
HARTING is the only 3D-MID manufacturer in the world that has a laser system with three fine-focus optics. The fine-focus laser can achieve even smaller trace spacing of only 70 to 80 µm. This enables many traces to be created on the same component so that a higher packing density can be reached.
3D-MID technology also allows for improved versatility in the shaping by creating flexible geometric contours in injection moulding and processing them with a laser for the electrical traces. Thus, rounded edges, elevations and transitions can also be created.

HARTING's security caps offer outstanding protection thanks to minimum trace spacing of 70 to 150 µm, more traces, and a higher packing density.

Lower costs thanks to automated production

HARTING's 3D-MID solutions are more secure. Moreover, thanks to the extensive automation of the entire supply chain, they are also more cost-effective than solutions from many other suppliers. All production steps are carried out at HARTING's own factory. This speeds up the process, increases the production yield and saves transportation costs. Even for products that are technologically less demanding, HARTING has been able to prevail over competitors from Asia.

Get in touch
Thomas Hess
Head of PM, Product & Technology Development