HANNOVER MESSE Press folder

All the information about the HANNOVER MESSE, from April 12-16, 2021, is included here.

Connectivity+: Powerful connectivity of the future

T1 industrial interface

The HARTING Technology Group is presenting itself with numerous technological highlights at this year's HANNOVER MESSE digital Edition (12 to 16 April 2021). "At HARTING, we are designing the powerful connectivity of the future and we call it Connectivity+," as CEO Philip Harting said. 

Download the full press release below to learn more. 

Download press material here:

Han® S gives users a complete cable assembly

Han® S

Energy efficiency is a topic that HARTING is concerned with and for which The HARTING Technology Group offers specific solutions: With its Han® S, HARTING has developed a series of connectors that enable customers to to build energy storage systems on the basis of battery modules. The Han®S is also the first HARTING-developed connector specifically designed for front-mounting energy storage systems.

Download the full press release below to learn more. 

Download press material here:

Faster wall-mounting for connectors

Han® HPR 16 B

The metal housings in the Han® EMV and Han® HPR series are now also available in versions that enable contact inserts to be mounted from the rear -- an option that simplifies the placement of interfaces on switch cabinet walls and and increases the installation speed and thus lowers costs in the long term.

Download the full press release below to learn more. 

Download press material here:

Han® L32 B offers optimal use of installation space

Han® L32

Using an L32 B connector allows users to replace two size 16 B interfaces -- saving over 40% of installation space. This makes it possible to transmit power, signals and data with fewer interfaces and fewer components.

Download the full press release below to learn more. 

Download press material here:

All-new system solutions for power distribution in rail vehicles

Han® HPR TrainPowerLine

HARTING has developed new interfaces for the power supply of trains that are optimized for a long service life and thus stand for sustainability.  This upcoming technology is called the the Han® HPR High Performance Transformer Connector (HPTC) and is a transformer interface especially developed for railway customers.

Download the full press release below to learn more. 

Download press material here:

New Han® modules for compressed air, energy storage and Ethernet

Han-Modular® pneumatic double module

In the Han-Modular® series, HARTING offers numerous connectors with which the energy efficiency of machines and systems can be sustainably increased. The latest example of this is the Han® 300 A module. It fits in with the classic development goal for for energy storage systems by enabling more capacity with less weight.

Download the full press release below to learn more. 

Download press material here:

RJ Industrial® MultiFeature facilitates access to the IIoT

RJ Industrial® MultiFeature

In 2021, HARTING once again exhibited at the digital HANNOVER MESSE (April 12- 6, 2021), highlighting the right infrastructure for the road to IIoT. Solutions such as the RJ Industrial®MultiFeature - a significantly improved version of the classic RJ45 in terms of in terms of handling. 

Download the full press release below to learn more. 

Download press material here:

har-modular®: Modules for power, signals and data – ideally combined 

har-modular®

Device development in the industrial arena is advancing in ever shorter cycles. At the same time, devices are becoming more and more compact, presenting challenges for developers looking for for the right solution for all the data, signals or power they need to transmit. Geared to facilitating the developers' work, HARTING is offering a solution with har-modular® that is opening up an entirely new scope of flexibility on PCBs.

Download the full press release below to learn more. 

Download press material here:

Get in touch
Christina Chatfield
Executive Vice President of Digital Strategy and Marketing Communications