INNOTRANS
Here you will find all information about INNOTRANS from September 20th to 23rd, 2022
“The Future of Mobility” is the theme of InnoTrans 2022 which will be held in Berlin from 20 to 23 September. After a break of four years, InnoTrans is opening its doors again and the HARTING Technology Group will also be on location and for the first time in Hall 16, Stand 200.
HARTING at InnoTrans 2022
Download press material here:
Han® HPR Compact
Download press material here:
Han-Modular® Domino Modules
With its Han-Modular® Domino modules, HARTING is taking modular connectors to the next level. The Domino system reduces the total number of interfaces required. The reason is that the connection technology is smaller and lighter – compared with interfaces with Han-Modular®. More module elements can fit into one connector than previously possible. For example, four different modular interfaces can now fit into a standard 6 B housing instead of the previous two.
Download press material here:
Han® HPR Single Poles
With its Han® HPR VarioShell, HARTING has developed a particularly flexible solution for jumper cable connections in rail vehicles. The housing forms an open system that can accommodate power connectors as well as other media. As the perfect complement, HARTING is launching the Han® HPR Single Poles which can transmit power up to 650 A / 4 kV AC/DC with its proven HC contacts.
Download press material here:
Press Contact
HARTING Stiftung & Co. KG
Detlef Sieverdingbeck
General Manager Communication and Public Relations
Marienwerderstr. 3
32339 Espelkamp
Tel.: 05772 47-244
Fax: 05772 47-400
Detlef.Sieverdingbeck(at)HARTING.com