Industrial technology leaders stand united behind IEC 63171-6

SPE Industrial Partner Network

SPE Industrial Partner Network

Single Pair Ethernet (SPE) is the infrastructure foundation that makes IIoT and Industry 4.0 possible. SPE offers, for the first time, the ability to use Ethernet cost-efficiently all the way to the field level with only one pair of wires. These and many other advantages make SPE the most important infrastructure innovation on the path to IIoT.

More information at www.single-pair-ethernet.com.

What is the Single Pair Ethernet Industrial Partner Network?

Seven of the leaders in industrial technology have joined forces to advance this technology for the rapidly growing IIoT market. HARTING, TE Connectivity, HIROSE, Würth Electronics, LEONI, MURR Elektronik and Softing are the founding members of the SPE Industrial Partner Network.

The SPE Industrial Partner Network is the first point of contact for users when they need to set up SPE networks and devices. This partnership provides clear recommendations for developing future IIoT applications, operates a central information platform, and provides investment security for users so they can rely on this technology in the future.

The security that users have in this investment is underlined by the rapid growth of the SPE network. As of March 2020, the technology companies Amphenol, Dehn, EKF, ESCHA, HELU Kabel, Hirschmann Automation, igus, Lütze, Metz Connect, Molex, Perinet, Zhaolong, Quabbin, Leviton and THK have also joined the partner network. Thus, there is a complete ecosystem of suppliers for infrastructure, Ethernet chips, magnetics, industrial devices and testing equipment.

More information at  www.single-pair-ethernet.com.

Expertise in the SPE ecosystem

With our T1 Industrial interface that is specially designed for SPE, we offer you the only true SPE interface for industrial applications supported by all international standards:

  • Standardized according to IEC 63171-6
  • Specified as an industrial interface by ISO/IEC SC25 WG3 and TIA42
  • Coordinated with cable and transmission standards, according to IEC 61156-x and IEEE 802.3.

Smaller, lighter and more robust The standard interface for your IIoT applications

Check out our YouTube video to find out more about Single Pair Ethernet:

Single Pair Ethernet (SPE) - explained easily: The Enabler for IIoT

As a founding member of the SPE Industrial Partner Network, we are one of the seven strong brands dedicated to providing you with a complete SPE ecosystem that enables you to implement this technology and pave your way to a true Internet of Things. As experts in connection technology, we are the proper people to get in touch with when you need to find the right contact.

T1 Industrial brings SPE into all IIoT applications – Intelligence to the edge!