Contact HARTING AE
Professionals Contact Intro Hero
HARTING Worldwide
HARTING Worldwide - Flags

Alternatives:

Search by series
Configurators
  1. Home
  2. News
  3. Han® S 450 Plus: Reliable and powerful connector for energy storage systems
Products
5 November 2025
2 minutes

Han® S 450 Plus: Reliable and powerful connector for energy storage systems


HARTING's battery connector series now supports up to 500 A for faster charging and discharging—ideal for high-performance energy storage without overheating.
Header_Product-News_Han-S-450-Plus.jpg

Energy storage systems (ESS) require interfaces that are compact and generate as little heat as possible, even when transmitting high currents. HARTING has developed the Han® S series for this application area. The cable side consists of angled housings, with the input side freely rotating around 360 degrees when plugged in. This makes the cables which connect the ESS modules more flexible. A maximum number of storage modules can be combined into larger units.

HARTING is presenting the new Han® S 450 Plus with contacts whose power capacity has been increased to 500 A. Until now, 200 A was the maximum power rating. The connector specialist is thus meeting the demand for higher charging and discharging currents for battery storage. The enlarged contacts and housings are designed so that they do not overheat during operation.

Specifically, HARTING has developed larger housings for contacts with three different conductor cross-sections:

  • for 95 mm² (AWG 3/0 or 4/0) up to 350 A

  • for 120 mm² (250 kcmil) up to 400 A

  • and for 150 mm² (300 kcmil) up to 450 A

The upper limit for the Han® S is certified at 450 A / 2000 VDC. This corresponds to the increased power requirements of up-to-date ESS. In the laboratory, the connector with a 150 mm² contact has already been successfully tested for direct current transmission at 500 A/2,000 VDC.

HARTING's energy storage connector series is thus returning to the top of the market in terms of current carrying capacity. Robustness and ease of use are also arguments in favour of the Han® interface: it is guaranteed to withstand up to 500 mating cycles, which no other comparable product can offer. The locking mechanism is intuitive.

The colours red for plus and black for minus, as well as additional colour options blue and orange, make Han® S connections absolutely confusion-proof. In addition, the housings feature a double locking system and numerous coding options, including the use of five different mating profiles. ‘No other connector in the market currently offers this level of security,’ says Product Manager Herman Liang from the HARTING Technology Group.

Han® S 450 Plus connectors on an energy storage cabinet

Han S 450_Sample_DSC3318.png

Product sample Han® S 450 Plus

Would you like to experience the new Han® S 450 Plus?
Request your free sample to get a first impression.

Request free product sample
Herman Liang (HARTING)

Herman Liang

Position: Global Product Manager

  • Company: HARTING Technology Group

Related news


2022-09_Verschwommene Lichter_Stadt_Straße_GettyImages-615429200.jpg
9 December 2025

Year in Review: Connectivity Trends Shaping 2025

As industries accelerate toward bringing new technologies to market, connectivity is emerging as a necessary catalyst for transformation. As we look back on the changes we saw across industrial connectivity, from hyperscale data centers to smart factories to modern power grids, here were the five trends that made the most impact ... and will continue making waves next year and beyond.
read more
Header_Product-News_Han-Contacts-on-Reel.jpg
5 November 2025

Faster processing of turned contacts

HARTING is launching a solution that processes turned contacts on reel to speed up cable assembly in semi-automatic and fully automatic crimping machines. High-quality contacts can thus be crimped onto conductors in a matter of seconds.
read more
Data Centre header background
23 October 2025

Building Smarter Data Center Infrastructure for the AI Age

Serving next-generation, AI-driven applications requires a dramatic rethink of traditional data center design. Data center infrastructure must evolve rapidly – becoming not only larger, but smarter, faster, and greener. Every connection system and square foot now counts in the race to keep up with exponential demand.
read more

HARTING Newsletter

Social Media


© HARTING Technology Group

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Customer Information