Contact HARTING AE
Professionals Contact Intro Hero
HARTING Worldwide
HARTING Worldwide - Flags

Alternatives:

Search by series
Configurators
  1. Home
  2. News
  3. Han® Size 4 saves up to 40% of installation space
Products
21 April 2026
3 minutes

Han® Size 4 saves up to 40% of installation space


New Size 4 connector solutions delivering high power density and space savings.
Han Size 4 saves up to 40% of installation space

Han-Eco®, Han® B and Han® HPR are the first connector series featuring Size 4 hoods/housings and inserts. This new size, an intermediary between Han® 3 and Han® 6, offers space savings of up to 40% compared to the next larger size. HARTING thus offers sustainable solutions for environments where installation space is limited to a minimum. There is a particular demand for this in mechanical engineering and automation as well as in energy and transportation applications.

Increase power density

The new size bridges a gap between two standards: the next-largest Han-Eco® 6B, for example, is not suitable for all energy applications, whilst the smaller Han® 3A cannot carry the required 70 A (the maximum is 40 A). Interfaces need to have a small footprint and must simultaneously transmit high currents, as capacities are rising and space is at a premium.

With the new size, users gain space for the rest of the required infrastructure, e.g., for cooling/ventilation. At the same time, the 70 A contacts of the Han-Eco® enable energy savings of up to 50%, which also promotes sustainability. This is primarily due to the low impedance of the silver-plated 70 A power contacts compared to competing products (CEE plugs).

Option for mechanical engineering and robotics

There is also demand for the new size in power distribution and transmission as well as in mechanical engineering. For instance, Size 4 hoods or housings and inserts allow space-saving connections for drives, frequency converters and other equipment to be installed in harsh industrial environments. Special adapters are available for integrating inserts from a range of over 100 different Han-Modular® connectors, including PE conductors.

Customer benefits at a glance:


  • Space saving connections for drives, frequency inverters and other devices in harsh industrial environments

  • Up to 40% reduction in installation space whilst maintaining the same performance

  • Improved sustainability through reduced material consumption whilst maintaining the same technical functionality

  • Scalable and future-proof due to a modular design featuring more than 100 different modular inserts

  • Easy PE-connection via tool-less Push-In termination technology

Han size 4B group

Han® Size 4 overview of metal and plastic versions

Press Kit: HANNOVER MESSE 2026 - Han® Size 4
Electric, Kontakt, Maik Iphöfer_20200826_DSC03191.jpg

Maik Iphoefer

Position: Product Manager

  • Department: PM Installation Technology
  • Company: HARTING Technology Group
Cuma Yuecel - HARTING

Cuma Yücel

Position: Product Manager

  • Department: PM Heavy Duty Connectors
  • Company: HARTING Technology Group

Related news


2024-09_robotic_engineers_GettyImages-2158997931.jpg
24 June 2026 Products

The industrial reality check – why factory winners execute, not just innovate

Manufacturers are operating in a moment where disruption is the norm, not the exception. Supply chain volatility, inflationary pressure and labor constraints all collide with a parallel push to embed automation and AI into plants that were never designed for today’s technologies.
read more
iStock-1481351307.jpg
21 May 2026 Products

The Industrial Reality Check: Why Factory Success Depends on Execution, Not Ambition

Execution means improving data visibility and equipment reliability incrementally, not waiting for a complete digital overhaul that may never come.
read more
News - Han 1A cable entry size 2
20 April 2026 Products

Han® 1A becomes more compact and powerful

Han® 1A expands application possibilities with higher currents and larger cable diameters.
read more

HARTING Newsletter

Social Media


© HARTING Technology Group

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Customer Information