Contact HARTING AE
Professionals Contact Intro Hero
HARTING Worldwide
HARTING Worldwide - Flags

Alternatives:

Search by series
Configurators
  1. Home
  2. News
  3. Han-Yellock® relaunch with reduced insertion forces
Products
20 April 2026
2 minutes

Han-Yellock® relaunch with reduced insertion forces


Redesigned Han Yellock® connector with reduced locking forces and enhanced usability.
yellock_2punkt0_header_news.jpg

HARTING has redesigned the Han-Yellock®: as a result, the versatile connector is now even easier to use. Locking forces have been significantly reduced.

The Han-Yellock® retains its traditional design, which combines black and melon yellow colours with attractive, rounded contours and zinc die-cast components. Changes have been made to the handling: gentle pressure on the buttons is all that is needed to release the connector. Narrow, circumferential double-lipped seals on the bulkhead-mounted housing and the carrier hood ensure lower locking forces.

“The Han-Yellock® is primarily used in exposed areas where good design and minimal installation height are required, such as in robotics,” reports Product Manager Tarek Spreen from HARTING Electric. Depending on the application, the Han-Yellock® also offers opportunities for miniaturisation. The power density is particularly high in the Han-Yellock® monoblocks. In the Han-Yellock® 60, 48 Yellock specific power contacts (16 A) can be fitted within an area comparable to the dimensions of a Han® 16B hood/housing. Using 25 contacts (16 A), the Han-Yellock® 30 monoblock exceeds the power density of Han® EE inserts in Han® 6B standard hoods/housings.

Han-Yellock® is a connector that combines a range of innovative solutions within an aesthetically pleasing overall design:

  • An audible ‘click’ indicates that the locking process is complete.

  • The cable side is divided into two parts, enabling front and rear mounting. The interfaces must not be separated for a visual inspection of the connection side.

  • Han-Yellock® multipliers allow contacts and potentials to be doubled.

  • Adapter frames allow for an easy integration of Han-Modular® modules.

  • 25 different coding options ensure that each connector is mounted in the correct position.

  • Shorter assembly times thanks to the snap-in option for Han-Modular® modules and Han-Yellock® monoblocks.

Customer benefits at a glance:


  • Easy handling due to reduced mating and locking forces

  • High contact density and bridging in a low construction interface

  • High mating cycles ensure a longer lifetime

  • Designed for applications with aesthetic requirements

Han-Yellock 60 and 30

Relaunched Han-Yellock® 30 (left) and 60 (right): ease of use, low insertion forces

To the products
Press Kit: HANNOVER MESSE 2026 - Han-Yellock®
Tarek Spreen

Tarek Spreen

Position: Product Manager

  • Department: Heavy Duty Connectors
  • Company: HARTING Technology Group

Related news


2024-09_robotic_engineers_GettyImages-2158997931.jpg
24 June 2026 Products

The industrial reality check – why factory winners execute, not just innovate

Manufacturers are operating in a moment where disruption is the norm, not the exception. Supply chain volatility, inflationary pressure and labor constraints all collide with a parallel push to embed automation and AI into plants that were never designed for today’s technologies.
read more
iStock-1481351307.jpg
21 May 2026 Products

The Industrial Reality Check: Why Factory Success Depends on Execution, Not Ambition

Execution means improving data visibility and equipment reliability incrementally, not waiting for a complete digital overhaul that may never come.
read more
Han Size 4 saves up to 40% of installation space
21 April 2026 Products

Han® Size 4 saves up to 40% of installation space

New Size 4 connector solutions delivering high power density and space savings.
read more

HARTING Newsletter

Social Media


© HARTING Technology Group

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Customer Information