Customised Machine Manufacturing
Customised Machine Manufacturing
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
HARTING Tech Day
TECH DAY DACH Header
Technical support
Customer Support - Front of HARTING plant 1 HQT
Returns & Complaints
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
Contact HARTING Austria
Professionals Contact Intro Hero
HARTING Worldwide
HARTING Worldwide - Flags

Alternatives:

Search by series
Configurators
  1. Home
  2. Hydrogen Technologies
  3. Hydrogen Utilization

Hydrogen utilization

As a pioneering energy carrier, hydrogen sets standards for emission-free and efficient energy generation. HARTING Connectivity supports this with solutions for the transmission of energy and data.


Hydrogen utilization

Hydrogen technologies play an important role in the energy transition and offer a wide range of potential applications. The hydrogen produced can be used in fuel cells to generate electrical energy. This process utilises so-called cold combustion, in which a controlled reaction of hydrogen with oxygen takes place in the fuel cell. This produces electrical voltage. The only by-product is pure water; no additional emissions are released.

Among other things, this technology is used in fuel cell vehicles, which represent an environmentally friendly alternative to conventional combustion engines.

Combined heat and power (CHP) plants can utilise hydrogen to generate electricity and heat at the same time. They are particularly important for decentralised energy supply. They offer an efficient solution for supplying energy to buildings and can help to stabilise the electricity grid.


In industry, hydrogen is used as a means of steel production to reduce CO2 emissions. Hydrogen is also used in other high-temperature processes to make industrial production more sustainable.


In addition, hydrogen is used in modified boilers or heating systems for environmentally friendly heat generation. This contributes to the reduction of greenhouse gas emissions and supports the transition to low-carbon building heating.


Research in the aviation and shipping sector shows the potential of hydrogen as a fuel that could lead to a significant reduction in greenhouse gas emissions. This would be a major step towards sustainable mobility.


In short, hydrogen technologies offer a wide range of applications that contribute to the decarbonisation of various sectors and support the energy transition. They are an essential component on the road to a sustainable and climate-friendly energy supply of the future.

Our expertise


Hydrogen production
Hydrogen storage and transport

Your Contact Person
FAQ

droplet-solid

Emission-free

Fuel cells produce energy with no harmful emissions, releasing only water as a byproduct.
Tachometer

Efficient

They convert chemical energy directly into electrical energy, offering a high level of efficiency.
ship

Versatile use

Fuel cells are used in vehicles, stationary energy systems, and portable devices.

Hydrogen fuel cell

Discover how HARTING products and solutions enhance fuel cell systems for hydrogen. Explore our application possibilities here:


Hydrogen Utilization - Landscape
Hydrogen Ecosystem FuelCell Poweroutput

Power Output efficient and powerful

HARTING products can be found in fuel cells, e.g. at the power output. The performance and efficiency of the connectors for high currents are important here. Due to their specification, HARTING Han® HPR Single Pole connectors are particularly suitable for powerful fuel cell systems. They achieve parameters of up to 650 A at 4 kV AC/DC and, with a degree of protection of IP68/69, offer a robust solution that functions reliably even in demanding environments.

Reliable power supply for peripheral systems (balance of plant)

The power supply for peripheral systems (Balance of Plant, BoP) - such as ventilation, pumps and cooling - is important for efficient operation. High-current connectors, the Han® S series, are used for this purpose. They offer a rated current of up to 450 A when using 150 mm² cables and reach voltages of up to 1500V DC. They have a degree of protection of IP67 and IP69K and are therefore ideal for harsh environments. Thanks to excellent vibration and shock resistance as well as ‘Touch Safe’ male and female contacts, they increase safety during operation.

Hydrogen Ecosystem FuelCell BoP
Hydrogen Ecosystem FuelCell ControlCabinet

Efficient communication and modular power supply

HARTING connectors make an important contribution to the transmission of power and data in fuel cells between the main control cabinet and the components of the fuel cell system - Balance of Plant (BoP). Important functions such as operating parameters (e.g. temperature, pressure, etc.) are monitored and controlled in the control cabinet. It is also where communication between the fuel cell and external control systems takes place. We offer modular connectors that enable communication between the control cabinet and the external control system and ensure their power supply. These modular solutions ensure efficient implementation and facilitate maintenance.

Interested? Get in touch with us!

If you are involved in the planning or manufacture of fuel cells and are looking for reliable connection solutions, please get in touch with us!


Interested? Get in touch with us!

Hydrogen News


Freighter at sea
30 March 2025

Charting the course to a green future

Ship propulsion with hydrogen: A project made for the eCap Marine GmbH from Hamburg
read more
Distrubution box for E-Cap Marine with Han-Ex.psd
15 January 2025

Connecting new energy with customer-specific solutions

Connectivity, i.e. the connection technology required for the transmission of data, signals and power, is playing a key role when it comes to the energy supply of the future.
read more

Your Contact Person


Bo Wang

Bo Wang

Position: Industry Segment Manager

  • Department: Industry Segment Management Energy
  • Company: HARTING Technology Group

Personal information

Contact information

Company

Address information

0/2000

By submitting the form you will send your request. HARTING Technology Group will then get in contact with you.

If you also confirm your e-mail address in an e-mail sent to you, you can subscribe to regular HARTING updates about events, news, products, and applications. You can unsubscribe at any time.

Hydrogen_Ecosystem_cropped-portrait_sRGB.tif

FAQ


Hydrogen is used in fuel cells to generate electrical energy through a controlled reaction with oxygen. This produces electrical voltage and the only by-product is pure water.

In industry, hydrogen is used as a reducing agent in steel production to reduce CO2 emissions. Hydrogen is also used in high-temperature processes to make industrial production more sustainable.

HARTING offers various solutions for fuel cells, including the Han® HPR single pole connectors, which can handle up to 650 A at 4 kV AC/DC and are IP68/69 protected. For the power supply of peripheral systems (balance of plant), the Han® S series connectors are ideal as they support up to 450 A and 1500 V DC and have IP67/IP69K protection. The connectors are vibration and shock resistant and offer additional safety thanks to their "Touch Safe" properties. In addition, HARTING's Han® industrial connectors and M12 circular connectors enable efficient communication and power supply between the main control cabinet and the external control system.

HARTING Newsletter

Social Media


© HARTING Technology Group

  • Imprint
  • Privacy Policy
  • Terms of Use
  • Customer Information