Maximizing Throughput for Semiconductor Manufacturers [Case Study]
HARTING is meeting miniaturization demands from chipmakers through connectivity
Meeting the Demands of the Semiconductor Boom
Never has there been greater pressure on
The Mandate: Do More in Less Space
These new initiatives create new demands for toolmakers that build the machines producing the chips. One such demand is to make their tools smaller to fit the maximum number in the fab. Another need is to increase the yield each tool produces, requiring integration of more technologies into a smaller space.
Doing more in less space feels like an impossible task, but through careful selection of subsystems, components and, most importantly, engineering partners, it is achievable. Top toolmakers are already accomplishing this.
Supplier Partnerships Are Crucial
Just as it takes a team to bring cutting-edge semiconductor tools from concept to production, it takes an ecosystem of expert suppliers to meet chipmakers' demands.
With one leading semiconductor tool manufacturing company, HARTING's expert connectivity teams were brought specific projects around the challenge of more output in less space. Challenge accepted.
Miniaturize Electrical Power Distribution Box While Simplifying Supply Chain
The Challenge
A major semiconductor equipment manufacturer needed to shrink an internal power distribution box on one of their tools to meet space-saving demands from end-users. Compliance with strict electrical and safety standards, fabrication requirements, precise spacing for varying wire thicknesses, safety for maintenance personnel, limited time, and space posed significant engineering challenges.
“We are extremely challenged from an engineering perspective,” said one of the engineers on the project. “If we cannot fit it, we have to change something about how space is allocated.”
The Solution
The manufacturer partnered with HARTING, utilizing
“HARTING’s diverse functionalities across its connectors makes it reliable, and we can apply it to all these products. Plus, it has extremely high configurability and is very easy to install. And in terms of the layout, it’s better because you have more opportunities in how you can allocate them within your canvas.”
Semiconductor toolmaker
Lead Engineer
Large-Scale Standardization and Customization Requirements
The Challenge
The same company returned to HARTING with a new challenge: expand standardization across a larger percentage of their power distribution box portfolio.
The previous designs used many connectors per box. Reducing the number of connection points would prevent against incorrect plugging as well as save space. However, they had a unique challenge they needed multiple different amperage options.
As the project progressed, the customer realized they needed a custom request related to the number of pins — all while keeping the project moving quickly.
The Solution
The HARTING team brought a solution that allowed them to use one module type to handle all amperages in a single
Regarding the custom pin count, HARTING was also able to address that quickly so that the toolmaker could stick to their promised timelines with the chipmaker.
Han® Modular Domino connectors provide function flexibility and free up valuable footprint.
Innovating Together
HARTING aims to be an extension of toolmaker’s engineer teams long term. HARTING has developed tools to help customers navigate the complex and often nuanced world of connectors no matter how the engineer wishes to design:
Self service design tools and comprehensive engineering product data that helps simplify an engineer’s workTravelling roadshow truck that brings the entire HARTING portfolio to an engineer’s doorstep
Collaborative design sessions and training tailored to your teams
In-region product development and manufacturing
On-site connectivity audits
Connect With Our Experts
Our team of Technical Application Consultants is available!
If you’ve got questions about connectorization or our solutions' capabilities, our experts are ready to answer them.
Contact our in-house engineers for technical guidance or design help and let us be the connector specialist extension of your team.