2. News
  3. Efficient data communication with Single Pair Ethernet
tec.news
April 19, 2026
5 minutes

Efficient data communication with Single Pair Ethernet


Experience how Single Pair Ethernet and intelligent sensor technology are revolutionising automation. Perinet enables direct data transmission from sensors through to IT levels – for efficient, future-proof production processes.
harting-web-2500x1500px-0084-Perinet-20260227.jpg
Karsten Walther_Porträt.jpg

Dr. Karsten Walther

Position: Managing Director

  • Company: Perinet GmbH

How IT is making its way into sensor technology


To date, there were the clearly separate worlds of the field level and higher-level IT. In the meantime, the two areas are now merging in terms of data technology. At the core of this development is the question as to how information can be transferred from the machine level to digital systems efficiently, comprehensibly and without media gaps. This is precisely where Perinet comes in with a novel approach that is dissolving traditional boundaries.

Barrier-free communication between IT and sensor technology


Traditional systems are based on proprietary bus systems and gateways that utilise data at field level and only translate it to IT when required. This process causes delays, media gaps and complex integration efforts. Perinet enables direct Ethernet-based communication from sensors through to the IT‑level.

This consistency is based on Single Pair Ethernet (SPE), a technology that brings Ethernet‑communication to the most compact devices. Today, modern microcontrollers enable computing power in sensor format; SPE complements these capabilities by providing a suitable, compact network interface.

Intelligence moving into sensors


As computing power trends upwards, the tasks and role of sensor technology are changing. Information is no longer provided as raw data, but as relevant information. A sensor that previously only output voltage is now supplying information directly that is relevant to decision-making – such as the fill level of a tank, for example.

This is creating an intelligent data flow that relieves burdens on IT and reduces network loads. Sensor technology is developing into the first processing level and forms the cornerstone as IT‑technology penetrates increasingly deeper into the field level.

The future of automation


The automation of the future will be holistic, with automation at field level and IT complementing each other.

  • Field level: Networked, intelligent sensors that pre-process, interpret and securely communicate data and automate the production process.

  • IT‑level: AI, machine learning and the data-based optimisation of processes.

While machine control used to form the sole core of automation, the innovative power is increasingly shifting to the IT level, where information can be evaluated across systems and processes can be optimised dynamically.

Practical example: Brownfields the easy way


The approach impresses with its strength demonstrated especially in brownfield systems. Instead of integrating different machine control systems which involves considerable input and effort, Perinet accesses the information directly at sensors – parallel to the existing PLC, without impacting on the ongoing operations.

In complex systems such as bottling lines, it is sufficient to read out a few specific data points to visualise throughput and rejects. Operators benefit from a minimum of installation input and effort, standardised infrastructures and risk-free retrofitting, even of decades old machines.

Connectors as enablers


The merging of IT and sensor technology also places new demands on connection technology. Hybrid connectors that combine power and data in one interface are becoming the foundation for modern automation. Just as USB brought about standardisation in IT, compact hybrid solutions – for example in the Single Pair Ethernet environment – are facing similar developments in the industrial area.

About Perinet


Perinet is a German technology company that directly interconnects sensors, actuators and IT‑systems. The solutions enable secure, end-to-end data communication from field devices to higher-level software and cloud systems. In this way, Perinet is creating the foundation for advanced, data-driven production environments while facilitating the use of AI in industry.

Discover all articles of tec.news issue 50
tec.news editorial team

tec.news editorial team

  • Company: HARTING Stiftung & Co. KG
[email protected]

Related news


Man and woman in automation production with robots
April 19, 2026 tec.news

Autonomy becomes a principle for success

In an interview with Prof. Kasper Hallenborg about new opportunities created by software-driven robotics, digital twins and decentralised intelligence – and why automation is being fundamentally rethought right now.
read more
green background with blue and green hexagons
April 19, 2026 tec.news

Efficient production with agent-based systems

Agent-based systems are revolutionising industrial production: they enable flexible matrix production, raise efficiency and transparency and adapt dynamically to new requirements.
read more
harting-web-2500x1500px-0093-Thomas Kaemper-20260227.jpg
April 19, 2026 tec.news

Autonomous production from order to delivery

Experience how HARTING is enabling consistent, flexible and transparent production thanks to MOM, AMR and ERP deployment. Boost efficiency and quality through automated processes and real-time data.
read more

Social Media


© HARTING Technology Group

  • Imprint
  • Privacy Policy
  • Cookie Policy
  • Terms of Use
  • Customer Information