Digital and innovative: HARTING has received the "Digital Champion" award from FOCUS MONEY and DEUTSCHLAND TEST. The technology group was also named the industry winner in the Electronic Components Manufacturer category.
CEO Philip Harting is delighted to receive the "Digital Champion" award.
The accolade is awarded to companies that are particularly well equipped to meet digital challenges, are at the cutting edge of technology and stand out in the industry thanks to their innovative strength.
The "Digital Champions 2025" study was conducted by the IMWF Institute for Management and Economic Development. The result: around 1000 companies were awarded the title "Digital Champion 2025". The prerequisite was that they achieved at least 60 points. HARTING shone as the industry winner with the highest score of 100 points, clearly setting itself apart from second place (93.5 points). "The future is digital! Digitalisation is an important lever for innovative strength and especially for the vision of a sustainable future," says Philip Harting, CEO of the technology group, delighted with the award.
The results were obtained via a survey and social listening. Between 1 January 2023 and 31 December 2024, several hundred million online data sources (including websites, forums, blogs, press releases and news sites) were analysed and questionnaires sent to the 15,000 largest German companies were evaluated.
Detlef Sieverdingbeck
Position: General Manager Corporate Communication & Branding
- Department: CCB
- Company: HARTING Stiftung & Co. KG