Can Installing Connectors Be Even Easier? New Video from HARTING Shows How with PushPull
Elgin, IL. November 2018 - HARTING just announced a new campaign for their PushPull product line. Dubbed as "Click & Go," the campaign focuses on the ease of use of the well-established PushPull line. At the center of the campaign is a short video that focuses on the HARTING PushPull connector "bringing to life" various applications in industrial environments. The film highlights why PushPull is the trusted, easy-to-use connector for many industrial applications.
The key technology for the PushPull connector is an internal locking mechanism that offers a robust and secure connection without the need for levers or twisting into place. This makes the connector extremely easy to install and uninstall, especially in hard-to-reach places. The connection technology is available in rectangular and circular form factors.
An audible click verifies when the connection is made. And with its small form factor, the HARTING PushPull enables miniaturization. Plastic hoods and housings are corrosion-resistant and approved for outdoor use.
Watch the full video and learn more at www.HARTING-USA.com/PushPullConnectors
Press Photo (see JPG attached)
About HARTING
The HARTING Technology Group, family owned and based in Germany, employs more than 4,300 people globally with subsidiaries and branch offices in 44 countries. With production facilities in Europe, Asia, and the Americas, the HARTING portfolio of connectivity solutions focuses on multiple levels, from the machine to the device and into the communication infrastructure. The U.S. facility in Elgin, Illinois is one of three HARTING locations that manufactures the HIS product line (HARTING Integrated Solutions - backplanes) and custom cable assemblies. HARTING also has custom cable assembly capabilities in Mexico and Brazil. The company’s core business is intelligent and high-performance connection technology. HARTING works in almost all industrial markets with a focus on requirements for robust, reliable connectivity solutions.
Media Contacts:
Christina Chatfield
VP Digital Strategy & Marketing Communications
HARTING North America
1370 Bowes Road
Elgin, IL 60123, USA
+1 (847) 717-9217
[email protected]
Julie Chatman
Marketing Comm. Specialist
HARTING North America
1370 Bowes Road
Elgin, IL 60123, USA
+1 (847) 717-9288
[email protected]